New in 2021: Our new range of CRs has gotten even bigger with the addition of the 185 — giving you more performance than ever offered by a vertical multistage pump. Now, you can bring greater efficiency, reliability and ease of use to more applications and processes. Read about how the new CR range saved one chemical plant $30,000 on water intake per year.
Because these new vertical multistage pumps can handle more than 1,000 gpm and 1,000 feet of head, you can use them in applications that previously required larger split-case and end-suction pumps. The new CR technology is better for processes such as:
The new CR line is even more robust than its forerunners, thanks to state-of-the-art technology in simulation design, materials, testing and production, with features designed to reduce pump downtime and lower operating costs.
The only regular maintenance needed is fast and easy, and can be done on-site — keeping costs low.
Every detail of the new CR line was designed for maximum energy efficiency, reducing kilowatts without sacrificing performance.
The new CR line continues the Grundfos tradition of modularity and customizability. With millions of possible variants, you can match your exact specification — whatever the application.
A recent case study explains how the new CR technology saved one chemical plant $30,000 per year on maintenance costs, while increasing efficiency and decreasing downtime. Fill out the form below to read the case study now.